Content-type: text/html; charset=UTF-8
Man page of INTRO
INTRO
Section: Misc. Reference Manual Pages (3LIBIIO)
Updated: 30 April 2026
Index
Return to Main Contents
NAME
libiio-1.0 - introduction to
libiio,
a library for interacting with the Linux
IIO
subsystem and devices
SYNOPSIS
#include <iio.h>
cc file.c
-liio
OPTIONS
The define
IIO_CHECK_REG
will warn if return values are not checked. Most
libiio
functions, if/when a failure occurs will return a negative error number.
this warning will ensure these error numbers are looked at. There is
nothing more frustraining than calling a function, debugging some hardware,
and then eventually realizing there was a typo in an attribute name.
This option will force libraries users to at least capture the return value.
cc file.c
-DIIO_CHECK_REG -liio
DESCRIPTION
libiio
is a library used to interface to the
Linux Industrial Input/Output (IIO)
Subsystem. The Linux
IIO
subsystem is intended to provide support for devices that in some sense
are analog to digital or digital to analog converters (ADCs, DACs). This
includes, but is not limited to ADCs, Accelerometers, Gyros, IMUs,
Capacitance to Digital Converters (CDCs), Pressure Sensors, Color,
Light and Proximity Sensors, Temperature Sensors, Magnetometers, DACs,
DDS (Direct Digital Synthesis), PLLs (Phase Locked Loops),
Variable/Programmable Gain Amplifiers (VGA, PGA), and RF transceivers.
You can use
libiio
natively on an embedded Linux target (local mode), or use libiio to
communicate remotely to that same target from a host Linux, Windows
or MAC over USB, Ethernet or Serial.
DATA TYPES
The library makes use of C structures and typedefs to promote portability,
and is known to run on various GNU/Linux distributions, macOS,
Windows, and mbed (via tiny-iiod). The main C structures are:
- iio_context_params
-
-
IIO context creation information
- iio_attr
-
Structure holding meta-data for an attribute
- iio_scan
-
Structure holding scanning information
- iio_context
-
Contains the representation of an IIO context
- iio_device
-
Represents a device in the IIO context
- iio_channel
-
Represents an input or output channel of a device
- iio_buffer
-
An input or output buffer, used to read or write samples
- iio_buffer_stream
-
An opened buffer ready for data streaming
- iio_block
-
A block of memory containing data samples
- iio_stream
-
A helper object to simplify reading/writing to a iio_buffer
- iio_event
-
Represents a IIO event.
- iio_data_format
-
Contains the format of a data sample.
LIST OF ROUTINES
The following routines are part of the library. Consult the Doxygen pages
for details on their operation (in the SEE ALSO section).
Functions for handling pointer-encoded errors
Index
- NAME
-
- SYNOPSIS
-
- OPTIONS
-
- DESCRIPTION
-
- DATA TYPES
-
- LIST OF ROUTINES
-
This document was created by
man2html,
using the manual pages.
Time: 05:46:30 GMT, April 30, 2026