Content-type: text/html; charset=UTF-8 Man page of iio_reg

iio_reg

Section: LibIIO Utilities (1)
Updated: 30 April 2026
Index Return to Main Contents
 

NAME

iio_reg - do a low level read or write to SPI or I2C register  

SYNOPSIS

iio_reg [ options ] <device> <register> [<value>]  

DESCRIPTION

iio_reg is a utility for debugging local or remote IIO devices. It should not be used by normal users, and is normally used by driver developers during development, or by end users debugging a driver, or sending in a feature request. It provides a mechanism to read or write SPI or I2C registers for IIO devices. This can be useful when troubleshooting IIO devices, and understanding how the Linux IIO subsystem is managing the device.

 

OPTIONS

-h, --help
Tells iio_reg to display some help, and then quit.
-V, --version
Prints the version information for this particular copy of iio_reg and the version of the libiio library it is using. This is useful for knowing if the version of the library and iio_reg on your system are up to date. This is also useful when reporting bugs.
-S, --scan [backends]
Scan for available IIO contexts, optional arg of specific backend(s) 'ip', 'usb' or 'ip,usb'. Specific options for USB include Vendor ID, Product ID to limit scanning to specific devices 'usb=0456:b673'. vid,pid are hexadecimal numbers (no prefix needed), "*" (match any for pid only) If no argument is given, it checks all that are available.
-u, --uri
The Uniform Resource Identifier (uri) for connecting to devices, can be one of:
ip:[address]
network address, either numeric (192.168.0.1) or network hostname
ip:
blank, if compiled with zeroconf support, will find an IIO device on network
usb:[device:port:instance]
normally returned from iio_reg -S
serial:[port],[baud],[settings]
which are controlled, and need to match the iiod (or tinyiiod) on the other end of the serial port.
[port]
is something like '/dev/ttyUSB0' on Linux, and 'COM4' on Windows.
[baud]
is is normally one of 110, 300, 600, 1200, 2400, 4800, 9600, 14400, 19200, 38400, 57600, 115200 [default], 128000 or 256000, but can vary system to system.
[settings]
would normally be configured as '8n1' this is controlled by:
data_bits:
(5, 6, 7, 8 [default], or 9)
parity_bits:
('n' none [default], 'o' odd, 'e' even, 'm' mark, or 's' space)
stop_bits:
(1 [default, or 2)
flow_control:
('0' none [default], 'x' Xon Xoff, 'r' RTSCTS, or 'd' DTRDSR)
local:
with no address part.
-T, --timeout <arg>
Context timeout in milliseconds. 0 = no timeout (wait forever). Default is 0.
 

RETURN VALUE

If the specified device is not found, a non-zero exit code is returned.

 

SEE ALSO

iio_attr(1), iio_info(1), iio_rwdev(1), iio_reg(1), libiio(3)

libiio home page: https://wiki.analog.com/resources/tools-software/linux-software/libiio

libiio code: https://github.com/analogdevicesinc/libiio

Doxygen for libiio https://analogdevicesinc.github.io/libiio/  

BUGS

All bugs are tracked at: https://github.com/analogdevicesinc/libiio/issues


 

Index

NAME
SYNOPSIS
DESCRIPTION
OPTIONS
RETURN VALUE
SEE ALSO
BUGS

This document was created by man2html, using the manual pages.
Time: 05:46:30 GMT, April 30, 2026