Content-type: text/html; charset=UTF-8
Man page of iio_attr
iio_attr
Section: LibIIO Utilities (1)
Updated: 30 April 2026
Index
Return to Main Contents
NAME
iio_attr - list IIO devices, and read/write device attributes
SYNOPSIS
iio_attr
[
options
]
-d [device] [attr] [value]
iio_attr
[
options
]
-c [device] [channel] [attr] [value]
iio_attr
[
options
]
-D [device] [attr] [value]
iio_attr
[
options
]
-C [attr]
iio_attr
[
options
]
-f -d|-c|-B|-D [device] [channel] [attr] [path]
iio_attr
-S <arg>
iio_attr
-h
DESCRIPTION
iio_attr
is a utility for displaying information about local or remote IIO devices.
By providing an optional value,
iio_attr
will attempt to write the new value to the attribute.
COMMANDS
- The iio_attr utility has a few main options, which control what the main utility of the application is.
-
- -d, --device-attr
-
Read and Write IIO device attributes
- -c --channel-attr
-
Read and Write IIO channel attributes
- -B --buffer-attr
-
Read and Write IIO Buffer attributes
- -C --context-attr
-
Read and Write IIO Context attributes
- -D --debug-attr
-
Read and Write IIO Debug attributes
- -h, --help
-
Tells
iio_attr
to display some help, and then quit.
- -V, --version
-
Prints the version information for this particular copy of
iio_attr
and the version of the libiio library it is using. This is useful for knowing if the version of the library and
iio_attr
on your system are up to date. This is also useful when reporting bugs.
- -S, --scan [backends]
-
Scan for available IIO contexts, optional arg of specific backend(s) 'ip', 'usb' or 'ip,usb'.
Specific options for USB include Vendor ID, Product ID to limit scanning to specific devices 'usb=0456:b673'.
vid,pid are hexadecimal numbers (no prefix needed), "*" (match any for pid only)
If no argument is given, it checks all that are available.
OPTIONS
- -u, --uri
-
The Uniform Resource Identifier
(uri)
for connecting to devices, can be one of:
-
- ip:[address]
-
network address, either numeric (192.168.0.1) or network hostname
- ip:
-
blank, if compiled with zeroconf support, will find an IIO device on network
- usb:[device:port:instance]
-
normally returned from
iio_attr -S
- serial:[port],[baud],[settings]
-
which are controlled, and need to match the iiod (or tinyiiod) on the other end of the serial port.
-
- [port]
-
is something like '/dev/ttyUSB0' on Linux, and 'COM4' on Windows.
- [baud]
-
is is normally one of 110, 300, 600, 1200, 2400, 4800, 9600, 14400, 19200, 38400, 57600, 115200 [default], 128000 or 256000, but can vary system to system.
- [settings]
-
would normally be configured as '8n1' this is controlled by:
-
- data_bits:
-
(5, 6, 7, 8 [default], or 9)
- parity_bits:
-
('n' none [default], 'o' odd, 'e' even, 'm' mark, or 's' space)
- stop_bits:
-
(1 [default, or 2)
- flow_control:
-
('0' none [default], 'x' Xon Xoff, 'r' RTSCTS, or 'd' DTRDSR)
- local:
-
with no address part.
- -T, --timeout <arg>
-
Context timeout in milliseconds. 0 = no timeout (wait forever). Default is 0.
- -w, --write-only
-
Do not readback on Writes
- -i, --input-channel
-
Filters channels by input channels only
- -o, --output-channel
-
Filters channels by output channels only
- -s, --scan-channel
-
Filters channels by scan channels only
- -I, --ignore-case
-
When pattern matching devices, channels or attributes, ignore case
- -g, --generate-code <arg>
-
Generate small C or python snippets that emulate what you are doing on the command line. Argument is a file name 'foo.c' or 'foo.py'
- -f, --input-file
-
Treat the trailing [value] argument as a path to a file. The file's raw bytes are written to the attribute via the _raw API variant, instead of writing [value] as a string. Cannot be combined with
-C
or
--generate-code,
and is rejected when used with wildcard matches. A short write (fewer bytes accepted than supplied) is reported as a WARNING on stderr.
RETURN VALUE
If the specified device is not found, a non-zero exit code is returned.
SEE ALSO
iio_attr(1),
iio_info(1),
iio_rwdev(1),
iio_reg(1),
libiio(3)
libiio home page:
https://wiki.analog.com/resources/tools-software/linux-software/libiio
libiio code:
https://github.com/analogdevicesinc/libiio
Doxygen for libiio
https://analogdevicesinc.github.io/libiio/
BUGS
All bugs are tracked at:
https://github.com/analogdevicesinc/libiio/issues
Index
- NAME
-
- SYNOPSIS
-
- DESCRIPTION
-
- COMMANDS
-
- OPTIONS
-
- RETURN VALUE
-
- SEE ALSO
-
- BUGS
-
This document was created by
man2html,
using the manual pages.
Time: 05:46:30 GMT, April 30, 2026