|
libiio 1.0
Library for interfacing with IIO devices
|
Data Structures | |
| struct | iio_channel |
| Represents an input or output channel of a device. More... | |
Functions | |
| __api __check_ret __pure const struct iio_device * | iio_channel_get_device (const struct iio_channel *chn) |
| Retrieve a pointer to the iio_device structure. | |
| __api __check_ret __pure const char * | iio_channel_get_id (const struct iio_channel *chn) |
| Retrieve the channel ID (e.g. voltage0) | |
| __api __check_ret __pure const char * | iio_channel_get_name (const struct iio_channel *chn) |
| Retrieve the channel name (e.g. vccint) | |
| __api __check_ret __pure const char * | iio_channel_get_label (const struct iio_channel *chn) |
| Retrieve the channel label (e.g. anglY) | |
| __api __check_ret __pure bool | iio_channel_is_output (const struct iio_channel *chn) |
| Return True if the given channel is an output channel. | |
| __api __check_ret __pure bool | iio_channel_is_scan_element (const struct iio_channel *chn) |
| Return True if the given channel is a scan element. | |
| __api __check_ret __pure unsigned int | iio_channel_get_attrs_count (const struct iio_channel *chn) |
| Enumerate the channel-specific attributes of the given channel. | |
| __api __check_ret __pure const struct iio_attr * | iio_channel_get_attr (const struct iio_channel *chn, unsigned int index) |
| Get the channel-specific attribute present at the given index. | |
| __api __check_ret __pure const struct iio_attr * | iio_channel_find_attr (const struct iio_channel *chn, const char *name) |
| Try to find a channel-specific attribute by its name. | |
| __api void | iio_channel_enable (const struct iio_channel *chn, struct iio_channels_mask *mask) |
| Enable the given channel. | |
| __api void | iio_channel_disable (const struct iio_channel *chn, struct iio_channels_mask *mask) |
| Disable the given channel. | |
| __api __check_ret bool | iio_channel_is_enabled (const struct iio_channel *chn, const struct iio_channels_mask *mask) |
| Returns True if the channel is enabled. | |
| __api __check_ret size_t | iio_channel_read (const struct iio_channel *chn, const struct iio_block *block, void *dst, size_t len, bool raw) |
| Demultiplex and convert the samples of a given channel. | |
| __api __check_ret size_t | iio_channel_write (const struct iio_channel *chn, struct iio_block *block, const void *src, size_t len, bool raw) |
| Convert and multiplex the samples of a given channel. | |
| __api void | iio_channel_set_data (struct iio_channel *chn, void *data) |
| Associate a pointer to an iio_channel structure. | |
| __api void * | iio_channel_get_data (const struct iio_channel *chn) |
| Retrieve a previously associated pointer of an iio_channel structure. | |
| __api __check_ret __pure enum iio_chan_type | iio_channel_get_type (const struct iio_channel *chn) |
| Get the type of the given channel. | |
| __api __check_ret __pure enum iio_modifier | iio_channel_get_modifier (const struct iio_channel *chn) |
| Get the modifier type of the given channel. | |
| __api void iio_channel_disable | ( | const struct iio_channel * | chn, |
| struct iio_channels_mask * | mask | ||
| ) |
Disable the given channel.
| chn | A pointer to an iio_channel structure |
| mask | The channels mask to manipulate |
| __api void iio_channel_enable | ( | const struct iio_channel * | chn, |
| struct iio_channels_mask * | mask | ||
| ) |
Enable the given channel.
| chn | A pointer to an iio_channel structure |
| mask | The channels mask to manipulate |
| __api __check_ret __pure const struct iio_attr * iio_channel_find_attr | ( | const struct iio_channel * | chn, |
| const char * | name | ||
| ) |
Try to find a channel-specific attribute by its name.
| chn | A pointer to an iio_channel structure |
| name | A NULL-terminated string corresponding to the name of the attribute |


| __api __check_ret __pure const struct iio_attr * iio_channel_get_attr | ( | const struct iio_channel * | chn, |
| unsigned int | index | ||
| ) |
Get the channel-specific attribute present at the given index.
| chn | A pointer to an iio_channel structure |
| index | The index corresponding to the attribute |


| __api __check_ret __pure unsigned int iio_channel_get_attrs_count | ( | const struct iio_channel * | chn | ) |
Enumerate the channel-specific attributes of the given channel.
| chn | A pointer to an iio_channel structure |


| __api void * iio_channel_get_data | ( | const struct iio_channel * | chn | ) |
Retrieve a previously associated pointer of an iio_channel structure.
| chn | A pointer to an iio_channel structure |


| __api __check_ret __pure const struct iio_device * iio_channel_get_device | ( | const struct iio_channel * | chn | ) |
Retrieve a pointer to the iio_device structure.
| chn | A pointer to an iio_channel structure |


| __api __check_ret __pure const char * iio_channel_get_id | ( | const struct iio_channel * | chn | ) |
Retrieve the channel ID (e.g. voltage0)
| chn | A pointer to an iio_channel structure |


| __api __check_ret __pure const char * iio_channel_get_label | ( | const struct iio_channel * | chn | ) |
Retrieve the channel label (e.g. anglY)
| chn | A pointer to an iio_channel structure |
NOTE: if the channel has no label, NULL is returned.
| __api __check_ret __pure enum iio_modifier iio_channel_get_modifier | ( | const struct iio_channel * | chn | ) |
Get the modifier type of the given channel.
| chn | A pointer to an iio_channel structure |


| __api __check_ret __pure const char * iio_channel_get_name | ( | const struct iio_channel * | chn | ) |
Retrieve the channel name (e.g. vccint)
| chn | A pointer to an iio_channel structure |
NOTE: if the channel has no name, NULL is returned.


| __api __check_ret __pure enum iio_chan_type iio_channel_get_type | ( | const struct iio_channel * | chn | ) |
Get the type of the given channel.
| chn | A pointer to an iio_channel structure |


| __api __check_ret bool iio_channel_is_enabled | ( | const struct iio_channel * | chn, |
| const struct iio_channels_mask * | mask | ||
| ) |
Returns True if the channel is enabled.
| chn | A pointer to an iio_channel structure |
| mask | A pointer to an iio_channels_mask structure |
| __api __check_ret __pure bool iio_channel_is_output | ( | const struct iio_channel * | chn | ) |
Return True if the given channel is an output channel.
| chn | A pointer to an iio_channel structure |


| __api __check_ret __pure bool iio_channel_is_scan_element | ( | const struct iio_channel * | chn | ) |
Return True if the given channel is a scan element.
| chn | A pointer to an iio_channel structure |
NOTE: a channel that is a scan element is a channel that can generate samples (for an input channel) or receive samples (for an output channel) after being enabled.


| __api __check_ret size_t iio_channel_read | ( | const struct iio_channel * | chn, |
| const struct iio_block * | block, | ||
| void * | dst, | ||
| size_t | len, | ||
| bool | raw | ||
| ) |
Demultiplex and convert the samples of a given channel.
| chn | A pointer to an iio_channel structure |
| block | A pointer to an iio_block structure |
| dst | A pointer to the memory area where the converted data will be stored |
| len | The available length of the memory area, in bytes |
| raw | True to read samples in the hardware format, false to read converted samples. |

| __api void iio_channel_set_data | ( | struct iio_channel * | chn, |
| void * | data | ||
| ) |
Associate a pointer to an iio_channel structure.
| chn | A pointer to an iio_channel structure |
| data | The pointer to be associated |

| __api __check_ret size_t iio_channel_write | ( | const struct iio_channel * | chn, |
| struct iio_block * | block, | ||
| const void * | src, | ||
| size_t | len, | ||
| bool | raw | ||
| ) |
Convert and multiplex the samples of a given channel.
| chn | A pointer to an iio_channel structure |
| block | A pointer to an iio_block structure |
| src | A pointer to the memory area where the sequential data will be read from |
| len | The length of the memory area, in bytes |
| raw | True if the samples are already in hardware format, false if they need to be converted. |