libiio 1.0
Library for interfacing with IIO devices
Loading...
Searching...
No Matches
Data Structures
Here are the data structures with brief descriptions:
 Ciio_attrStructure holding meta-data for an attribute
 Ciio_bufferAn input or output buffer, used to read or write samples
 Ciio_buffer_streamAn opened buffer ready for data streaming
 Ciio_channelRepresents an input or output channel of a device
 Ciio_contextContains the representation of an IIO context
 Ciio_context_paramsIIO context creation information
 Ciio_data_formatContains the format of a data sample
 Ciio_deviceRepresents a device in the IIO context
 Ciio_eventRepresents a IIO event