|
C# bindings for libiio 1.0
C# bindings for libIIO
|
| Ciio.Attr | iio.Attr class: Contains the representation of an iio_attr |
| Ciio.BufferStream | iio.BufferStream class: The class used for streaming operations on opened buffers |
| Ciio.Channel | iio.Channel class: Contains the representation of an input or output channel |
| Ciio.Context | iio.Context class: Contains the representation of an IIO context |
| ▼Ciio.Device | iio.Device class: Contains the representation of an IIO device |
| Ciio.Trigger | iio.Trigger class: Contains the representation of an IIO device that can act as a trigger |
| Ciio.EventStream | iio.EventStream class: Contains the representation of an event stream |
| Ciio.IioContextParams | Represents the parameters for creating an IIO context |
| Ciio.IIOEvent | iio.IIOEvent class: Contains the representation of an iio_event |
| Ciio.IOBuffer | iio.IOBuffer class: The class used for all I/O operations |
| Ciio.Scan | iio.ScanContext class: Class for getting information about the available contexts |