C# bindings for libiio 1.0
C# bindings for libIIO
Loading...
Searching...
No Matches
iio.Trigger Class Reference

iio.Trigger class: Contains the representation of an IIO device that can act as a trigger. More...

Inheritance diagram for iio.Trigger:
Collaboration diagram for iio.Trigger:

Public Member Functions

void set_rate (ulong rate)
 Configure a new frequency for this trigger.
 
ulong get_rate ()
 Get the currently configured frequency of this trigger.
 
new void set_trigger (Trigger trig)
 Set Trigger.
 
new Trigger get_trigger ()
 Get trigger.
 
- Public Member Functions inherited from iio.Device
Channel get_channel (string name, bool output=false)
 Get the iio.Channel object of the specified name.
 
void set_trigger (Trigger trig)
 Affect a trigger to this device.
 
Trigger get_trigger ()
 Get the current trigger affected to this device.
 
uint get_sample_size (ChannelsMask mask)
 Get the current sample size of the device.
 
void reg_write (uint addr, uint value)
 Set a value to one register of this device.
 
uint reg_read (uint addr)
 Read the content of a register of this device.
 

Additional Inherited Members

- Public Attributes inherited from iio.Device
readonly Context ctx
 Gets the context of the current device.
 
readonly string id
 An identifier of this device.
 
readonly string name
 The name of this device.
 
readonly List< Attrattrs
 A list of all the attributes that this device has.
 
readonly List< Attrdebug_attrs
 A list of all the debug attributes that this device has.
 
readonly List< Channelchannels
 A list of all the iio.Channel objects that this device possesses.
 
readonly List< IOBufferbuffers
 A list of all the iio.IOBuffer objects that this device possesses.
 
- Properties inherited from iio.Device
string label [get]
 The label of this device.
 
bool hwmon [get]
 True if the device is a hardware monitoring device, False if it is a IIO device.
 

Detailed Description

iio.Trigger class: Contains the representation of an IIO device that can act as a trigger.

Examples
ExampleProgram.cs.

Member Function Documentation

◆ get_rate()

ulong iio.Trigger.get_rate ( )
inline

Get the currently configured frequency of this trigger.

Exceptions
IioLib.IIOExceptionThe configured frequency could not be obtained.
Here is the call graph for this function:

◆ set_rate()

void iio.Trigger.set_rate ( ulong  rate)
inline

Configure a new frequency for this trigger.

Exceptions
IioLib.IIOExceptionThe new frequency could not be set.
Here is the call graph for this function:

The documentation for this class was generated from the following file: