C# bindings for libiio 1.0
C# bindings for libIIO
Loading...
Searching...
No Matches
iio.IIOEvent Class Reference

iio.IIOEvent class: Contains the representation of an iio_event. More...

Collaboration diagram for iio.IIOEvent:

Public Types

enum  EventType {
  IIO_EV_TYPE_THRESH , IIO_EV_TYPE_MAG , IIO_EV_TYPE_ROC , IIO_EV_TYPE_THRESH_ADAPTIVE ,
  IIO_EV_TYPE_MAG_ADAPTIVE , IIO_EV_TYPE_CHANGE , IIO_EV_TYPE_MAG_REFERENCED , IIO_EV_TYPE_GESTURE ,
  IIO_EV_TYPE_FAULT
}
 iio.IIOEvent.EventType class: Contains the available event types.
 
enum  EventDirection {
  IIO_EV_DIR_EITHER , IIO_EV_DIR_RISING , IIO_EV_DIR_FALLING , IIO_EV_DIR_NONE ,
  IIO_EV_DIR_SINGLETAP , IIO_EV_DIR_DOUBLETAP , IIO_EV_DIR_FAULT_OPENWIRE
}
 iio.IIOEvent.EventDirection class: Contains the available event directions.
 

Public Attributes

readonly Channel chn
 
readonly Channel chn_diff
 
readonly ulong id
 
readonly long timestamp
 

Properties

EventType type [get]
 The type of this event.
 
EventDirection direction [get]
 Represents the direction of the event.
 

Detailed Description

iio.IIOEvent class: Contains the representation of an iio_event.


The documentation for this class was generated from the following file: