|
C# bindings for libiio 1.0
C# bindings for libIIO
|
This is the complete list of members for iio.Device, including all inherited members.
| attrs | iio.Device | |
| buffers | iio.Device | |
| channels | iio.Device | |
| ctx | iio.Device | |
| debug_attrs | iio.Device | |
| get_channel(string name, bool output=false) | iio.Device | inline |
| get_sample_size(ChannelsMask mask) | iio.Device | inline |
| get_trigger() | iio.Device | inline |
| hwmon | iio.Device | |
| id | iio.Device | |
| label | iio.Device | |
| name | iio.Device | |
| reg_read(uint addr) | iio.Device | inline |
| reg_write(uint addr, uint value) | iio.Device | inline |
| set_trigger(Trigger trig) | iio.Device | inline |