iio.Context class: Contains the representation of an IIO context.
More...
Inherits iio.IIOObject.
|
|
readonly string | xml |
| | A XML representation of the current context.
|
| |
|
readonly string | name |
| | The name of the current context.
|
| |
|
readonly string | description |
| | Retrieve a human-readable information string about the current context.
|
| |
|
readonly Version | library_version |
| | Retrieve a information about the version context.
|
| |
|
readonly Version | backend_version |
| |
|
readonly List< Device > | devices |
| | A List of all the IIO devices present on the current context.
|
| |
|
|
Dictionary< string, string > | attrs [get] |
| | A Dictionary of all the attributes of the current channel. (key, value) = (name, value)
|
| |
iio.Context class: Contains the representation of an IIO context.
- Examples
- ExampleProgram.cs.
◆ Context() [1/2]
Initializes a new instance of the iio.Context class using the specified context parameters.
- Parameters
-
| contextParams | The parameters used to configure the IIO context. |
| uri | URI to use for the IIO context creation |
- Returns
- an instance of the iio.Context class
- Exceptions
-
| IioLib.IIOException | The IIO context could not be created. |
◆ Context() [2/2]
| iio.Context.Context |
( |
string |
uri = null | ) |
|
|
inline |
Initializes a new instance of the iio.Context class, using the provided URI. For compatibility with existing code, providing an IP address or a hostname here will automatically create a network context.
- Parameters
-
| uri | URI to use for the IIO context creation |
- Returns
- an instance of the iio.Context class
- Exceptions
-
| IioLib.IIOException | The IIO context could not be created. |
◆ get_device()
| Device iio.Context.get_device |
( |
string |
name | ) |
|
|
inline |
Get the iio.Device object of the specified name.
- Parameters
-
| name | Name or ID of the device to look for |
- Exceptions
-
| IioLib.IIOException | The IIO device with the specified name or ID could not be found in the current context. |
◆ GetContextParams()
Retrieves the parameters of the current IIO context.
- Returns
- An instance of IioContextParams representing the context parameters.
- Exceptions
-
| IioLib.IIOException | Thrown if the parameters could not be retrieved. |
◆ set_timeout()
| void iio.Context.set_timeout |
( |
uint |
timeout | ) |
|
|
inline |
Set a timeout for I/O operations.
- Parameters
-
| timeout | The timeout value, in milliseconds |
- Exceptions
-
| IioLib.IIOException | The timeout could not be applied. |
The documentation for this class was generated from the following file: