|
C# bindings for libiio 1.0
C# bindings for libIIO
|
iio.Channel class: Contains the representation of an input or output channel. More...

Public Types | |
| enum | ChannelModifier { IIO_NO_MOD , IIO_MOD_X , IIO_MOD_Y , IIO_MOD_Z , IIO_MOD_X_AND_Y , IIO_MOD_X_AND_Z , IIO_MOD_Y_AND_Z , IIO_MOD_X_AND_Y_AND_Z , IIO_MOD_X_OR_Y , IIO_MOD_X_OR_Z , IIO_MOD_Y_OR_Z , IIO_MOD_X_OR_Y_OR_Z , IIO_MOD_LIGHT_BOTH , IIO_MOD_LIGHT_IR , IIO_MOD_ROOT_SUM_SQUARED_X_Y , IIO_MOD_SUM_SQUARED_X_Y_Z , IIO_MOD_LIGHT_CLEAR , IIO_MOD_LIGHT_RED , IIO_MOD_LIGHT_GREEN , IIO_MOD_LIGHT_BLUE , IIO_MOD_QUATERNION , IIO_MOD_TEMP_AMBIENT , IIO_MOD_TEMP_OBJECT , IIO_MOD_NORTH_MAGN , IIO_MOD_NORTH_TRUE , IIO_MOD_NORTH_MAGN_TILT_COMP , IIO_MOD_NORTH_TRUE_TILT_COMP , IIO_MOD_RUNNING , IIO_MOD_JOGGING , IIO_MOD_WALKING , IIO_MOD_STILL , IIO_MOD_ROOT_SUM_SQUARED_X_Y_Z , IIO_MOD_I , IIO_MOD_Q , IIO_MOD_CO2 , IIO_MOD_VOC , IIO_MOD_LIGHT_UV , IIO_MOD_LIGHT_DUV , IIO_MOD_PM1 , IIO_MOD_PM2P5 , IIO_MOD_PM4 , IIO_MOD_PM10 , IIO_MOD_ETHANOL , IIO_MOD_H2 , IIO_MOD_O2 , IIO_MOD_LINEAR_X , IIO_MOD_LINEAR_Y , IIO_MOD_LINEAR_Z , IIO_MOD_PITCH , IIO_MOD_YAW , IIO_MOD_ROLL , IIO_MOD_LIGHT_UVA , IIO_MOD_LIGHT_UVB , IIO_MOD_RMS , IIO_MOD_ACTIVE , IIO_MOD_REACTIVE , IIO_MOD_APPARENT } |
| iio.Channel.ChannelModifier class: Contains the available channel modifiers. | |
| enum | ChannelType { IIO_VOLTAGE , IIO_CURRENT , IIO_POWER , IIO_ACCEL , IIO_ANGL_VEL , IIO_MAGN , IIO_LIGHT , IIO_INTENSITY , IIO_PROXIMITY , IIO_TEMP , IIO_INCLI , IIO_ROT , IIO_ANGL , IIO_TIMESTAMP , IIO_CAPACITANCE , IIO_ALTVOLTAGE , IIO_CCT , IIO_PRESSURE , IIO_HUMIDITYRELATIVE , IIO_ACTIVITY , IIO_STEPS , IIO_ENERGY , IIO_DISTANCE , IIO_VELOCITY , IIO_CONCENTRATION , IIO_RESISTANCE , IIO_PH , IIO_UVINDEX , IIO_ELECTRICALCONDUCTIVITY , IIO_COUNT , IIO_INDEX , IIO_GRAVITY , IIO_POSITIONRELATIVE , IIO_PHASE , IIO_MASSCONCENTRATION , IIO_DELTA_ANGL , IIO_DELTA_VELOCITY , IIO_COLORTEMP , IIO_CHROMATICITY , IIO_ATTENTION , IIO_ALTCURRENT , IIO_CHAN_TYPE_UNKNOWN = Int32.MaxValue } |
| iio.Channel.ChannelType class: Contains the available channel types. | |
Public Member Functions | |
| void | enable (ChannelsMask mask) |
| Enable the current channel, so that it can be used for I/O operations. | |
| void | disable (ChannelsMask mask) |
| Disable the current channel. | |
| bool | is_enabled (ChannelsMask mask) |
| Returns whether or not the channel has been enabled. | |
| byte[] | read (Block block, bool raw=false) |
| Extract the samples corresponding to this channel from the given iio.Block object. | |
| uint | write (Block block, byte[] array, bool raw=false) |
| Write the specified array of samples corresponding to this channel into the given iio.Block object. | |
Public Attributes | |
| readonly Device | dev |
| readonly string | name |
| The name of this channel. | |
| readonly string | id |
| An identifier of this channel. | |
| readonly uint | index |
| Get the index of this channel. | |
| readonly bool | output |
Contains true if the channel is an output channel, false otherwise. | |
| readonly bool | scan_element |
Contains true if the channel is a scan element, false otherwise. | |
| readonly List< Attr > | attrs |
A list of all the attributes that this channel has. | |
Properties | |
| string | label [get] |
| The label of this channel. | |
| ChannelModifier | modifier [get] |
| The modifier of this channel. | |
| ChannelType | type [get] |
| The type of this channel. | |
| DataFormat | format [get] |
| Represents the format of a data sample. | |
iio.Channel class: Contains the representation of an input or output channel.
|
inline |
Extract the samples corresponding to this channel from the given iio.Block object.
| block | A valid instance of the iio.Block class. |
| raw | If set to true, the samples are not converted from their hardware format to their host format. |
byte array containing the extracted samples.| IioLib.IIOException | The samples could not be read. |
|
inline |
Write the specified array of samples corresponding to this channel into the given iio.Block object.
| block | A valid instance of the iio.Block class. |
| array | A byte array containing the samples to write. |
| raw | If set to true, the samples are not converted from their host format to their native format. |
| IioLib.IIOException | The samples could not be written. |
| readonly string iio.Channel.id |
An identifier of this channel.
It is possible that two channels have the same ID, if one is an input channel and the other is an output channel.
| readonly bool iio.Channel.scan_element |
Contains true if the channel is a scan element, false otherwise.
If a channel is a scan element, then it is possible to enable it and use it for I/O operations.