C# bindings for libiio 1.0
C# bindings for libIIO
Loading...
Searching...
No Matches
Class List
Here are the classes, structs, unions and interfaces with brief descriptions:
[detail level 12]
 Niio
 CAttriio.Attr class: Contains the representation of an iio_attr
 CBufferStreamiio.BufferStream class: The class used for streaming operations on opened buffers
 CChanneliio.Channel class: Contains the representation of an input or output channel
 CContextiio.Context class: Contains the representation of an IIO context
 CDeviceiio.Device class: Contains the representation of an IIO device
 CEventStreamiio.EventStream class: Contains the representation of an event stream
 CIioContextParamsRepresents the parameters for creating an IIO context
 CIIOEventiio.IIOEvent class: Contains the representation of an iio_event
 CIOBufferiio.IOBuffer class: The class used for all I/O operations
 CScaniio.ScanContext class: Class for getting information about the available contexts
 CTriggeriio.Trigger class: Contains the representation of an IIO device that can act as a trigger